This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5825M: THD+N of OUTPUT at high frequency is failed.

Part Number: TAS5825M


TROUBLE: With AP525, I check the output signal. THD+N at high frequency(higher than 3K) is more than 0.8%, but it is only 0.08% wih the same level at 1KHz.

Cause to find:

1. check THD+N of the input I2S signal , it's only 0.03%.

2. check the output with no load, it's 0.5%.

3. check before the LC filter, it's 0.4%.

4. check without LC or load, it's 0.35%

Could you please tell me how to do next? Is there anything to check with the firmware?

Thank you.