Hi!
my customer uses PCM1774 and has the following questions:
------------------------------------------------------------------
PCM1774 is used associated with a Silicon Lab CP2114.
The CP2114 generates 3 clocks to the PCM1774.
- One clock MCLK at 12MHz connected to the input SCKI of the PCM1774
- One clock SCK at 48MHz/14=3.428MHz connected to the input BCK of the PCM1774
- One clock LRCK at 12MHz/250=48kHz connected to the input LRCK of the PCM1774
What is the good setting for the register @ 0x55 ? (NPR[5:0] register).
We set this register to 0x04h (00 0100).
Is it the good setting for this register ?
In the PCM1774 what is called the sampling rate ?
--------------------------------------------------------------
Kind regards,
Marion