Other Parts Discussed in Thread: TAS5711, TAS5825M, TAS5805M
Hello,
New to hardware DSP development, but I work with some very smart and capable engineers.
Here's where I'm at:
We are creating a product featuring TAS5731
I am programming the DSP for it using the GDE. I am easily able to make a proper connection with my eval board to make and save parameter settings as PFW.
This all works mostly as expected.
The issue I am having currently is two fold.
Issue 1: A setting is showing 1.0, but actually calculating 0.0
That setting is Mix52/Mixer_0
Steps to reproduce issue
1. Load PFW
2. Note Setting of Mix52/Mixer_0 (It is 1.0)
3. Simply re-type 1.0 over the top of this setting
4. Channel assignment will respond appropriately. (In this case, the setting allows for mono channel operation - without it, one channel is not mono summed)
5. Re-load PFW, setting will again say 1.0 but not actually calculate 1.0 until you re-type in 1.0
6. Repeat until head explodes.
Expected Behavior:
The setting displaying 1.0 should calculate 1.0 after recalling PFW settings.
Are there other settings doing this?
Issue 2
My GDE shows TAS5711 as the "Current Device"- is this a problem?
Will I have settings translation issues if I burn these to production hardware?
Thanks, happy to provide more info.