This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3123D2 problem

Other Parts Discussed in Thread: TPA3123D2, PCM1754

Hi

I would like to design a audio system using TPA3123D2.

Output is BTL mode 50W output at 1% THD+N load is 8 ohm and input voltage is 30V.

However, TPA3123D2 input is connect to PCM1754 which should be single end output.

The design is suitable or any better suggestion.

 

BRs

 

Michael