Part Number: PCM1774
Hi,
my customer uses two PCM1774 and has the following questions:
Reading the datasheet I was not able to found a register that configure the PCM1774 output as a line output (load > 10kΩ) or a Headphone output (load 16Ω or 32Ω).
Q1: Is there a special register setting to select between LOL/LOR and HPOL/HPOR ?
Reading the datasheet page 3/4 Electrical Characteristic we found: 0dB gives 1Vrms typical at the output with a load of 10kΩ.
But we have done some measurement with all the registers on the PCM1774 set to 0dB, and we have about 750mVrms at the output with a load of 10kΩ.
Q2: why this difference between our measurements and the datasheet ?
Thank you for your help,
kind regards,
Marion