Hello
When not using the following pins, are the following pin treatments appropriate?
RXIN0, RXIN1: Not connected
RXIN2 to RXIN3: Direct connection to GND
RXIN4 to RXIN7: Direct connection to GND
MPIO_A0 to MPIO_A3: Directly connected to GND
MPIO_B0 to MPIO_B3: Directly connected to GND
MPIO_C0 to MPIO_C3: Directly connected to GND
VINL, VINR: Not connected
VCCAD: Directly connected to GND
VCOM: Directly connected to GND
Best regards,