Part Number: TAS5805MEVM
Other Parts Discussed in Thread: TAS5805M
I have configured the board in dual mono mode. One is driving a woofer, the other a tweeter. Sometimes everything works fine, but it is very easy to get the card to stop working. This seems related to the output power. The higher the peaks are, the easier it is to get it to stop working. I am running it on a lab power supply of 20V 5A. The load is sometimes 4 ohm speakers and sometimes power resistors (8 ohm each with max 300W).
Is there anything that I should do to prevent this from happening?
Any advice would be appreciated.
/Björn Gröhn