Part Number: TPA3116D2
Can I connect 4Ohm or 8Ohm drivers to the TPA3116D2 in mono mode? What will the maximum power? Will it hold 50W at 8Ohm?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPA3116D2
Can I connect 4Ohm or 8Ohm drivers to the TPA3116D2 in mono mode? What will the maximum power? Will it hold 50W at 8Ohm?
Paleari,
Yes, your can connect 4ohm/8ohm in Mono mode.
About the maximum power, with 4ohm/8ohm load, the mono mode output power is same as stero mode. because maximum output power limitation is not device current capability. So you can refer datasheet Figure 13 and 14 to find the maximum output power.
Dylan