This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5630B: what will result in SD active?

Part Number: TAS5630B


Hi,

customer use our TAS5630B and meet issue about SD active.

same sch with datasheet as below.

1 no resistor between OUT_X and GND_X and PVDD_X.

2 power supply PVDD=50Vvdd=12V,

3 no thermal protection.

4 break load, get the same results-- no output and SD active.

5 manually change RESET status, no change

6 change another device, SD normal but still no output.

Do you have any suggestion on that? it's an urgent issue, need your support.

thanks.

Yuan

  • Hi,

    Please make sure customer's schematic is the same with the reference design on datasheet, and check below points,

    1. When pulling the RESET# high, please check the voltage on VREG /VI_CM /C_startup/, and check if there is any switching on OUTx.

    2. When pulling the RESET# low, please check voltage on SD#. It should be logic high.

    3. If SD status changed with the replacement of a new device, please check if there is any problem with the soldering.

    Regards,

    Sam

  • Hi Sam,

    thank you!

    here is the feedback:

    1. when reset high, VREG(~3.2V) /VI_CM (1.94V)/C_startup(3.1V),no output.
    2. when IC alert, no matter reset is high or low, SD keep low;
    3. customer changed 5 ICs, all appears SD alert after different working time;
    4. their load is soundwave motor,  the voltage of motor is -25V~+25V. sine wave.
    5. drive signal is 3~100Hz, is that OK for this part?

       thank you!

    Yuan

  • Hi Yuan,

    1. VREG/ VI_CM/ C_start voltages are normal.

    2. Once Reset# is pulled low, SD will be forced to high. Refer to bottom of page 17 on d/s. If SD# pin is always low, please check if the device is good unit and the soldering.

    3. So the device can work normally for some time, right? Under what working condition did the device fall into fault status? Is it delivering high power? 

    4. This device is an audio amp that may have some limitations to support frequency as low as 3Hz. At least it won't work with current  How about the loading condition?

    Regards,

    Sam

  • Hi Sam,

    thanks for your support.

    the load is maximum 357W.

    and here is the schematics:

    Power amplifier board V0.1.pdf

  • Hi,

    The schematic looked good.

    1. First of all, please make sure that when RESET# pulled low, SD# was in high level. If it is not, please check the soldering. 

    2. You may also refer to Table 1 in datasheet to check what kind of fault it's reporting.

    3. What's the load resistance? The device has current limit as 15A, and can support ~350W on at least 3R loading. With lower loading resistance, it may trigger over current fault.

    Regards,

    Sam

  • Hi Sam,

    7R loading.

    when IC works, assert reset low, SD high. but when SD alert, it keeps low whether reset is high or low.

    why? does it mean that the IC is broken?

    thank you!

    Yuan

  • Hi Yuan,

    I can't tell the IC is damaged, but according to the datasheet, asserting reset low should make SD released to high level, independent of faults being present.

    BTW, if the loading is 7R, we can't get 375W output. The max output we can support without a voltage clipping, is 50^2/2/7=178W. With 10% THD+N, it can support about 200W.

    Regards,

    Sam