This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The gain of TAS5782 is 6db lower than the actual setting. For example, when we set it to 0db, it was actually measured to be -6db. We also tested it with TAS5782MEVM.Where will the PWM frequency and gain be affected?
Hello customer,
It is suggested to do experiments on EVM with GUI. Then check:
If every gain is ok, it should not be -6dB lower. Please try to input -30dBFS and 0dBFS for check.
Regards,
Alix Wan.
Hello customer,
For TAS5782 itself, if your configuration of Fsw=768K and gain =26dB, it won't change except SPK_GAIN in table 14 is affected by external circuit. Hence, may you:
Please do a comparison when output power is normal vs abnormal. Thanks!
Regards,
Alix Wan.