Other Parts Discussed in Thread: TPA3250,
Hello,
The board always play for 5 seconds and shutdown. It report fault only (otw light not on)
Could you help check what the matter is?
Regards,
Louie LI
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Louie,
Can you give us more details of your system?
- impedance of the load/speaker
- I tried looking at what type of inductor you are using but it was in chinese. Do you have the datasheet for it?
Regards,
Robert Clifton
Hi Louie,
So does the device shutdown whether you are playing audio or not? If you turn the volume down do you see the same shutdown?
Another thing I don't see is the inductance curve vs current for the inductor. If the inductance drops below 5uH then the amplifier can shutdown since the minimum expected impedance is violated.
Regards,
Robert Clifton
Robert,
Thank you! I'll do these tests later to see if it still goes into a fault mode in those circumstances.
Another problem I met is TPA3250 shutdown. Two sample boards meet the problem that when I press the chip, it works but when I stop pressing it it goes into a fault mode,
I suspect it is because manufacturer use high temperature and injures the chip but not sure. I am now trying to reassemble boards to check it. If there is any useful information, appreciate if you share with me.
Regards,
Louie LI
Hi Louie,
So you are also using a TPA3250?
This sounds like there wasn't a good connection between the thermal pad and the PCB since this is a pad down device. This does sound like a thermal issue from your description. Under what conditions are you testing the device under?
Regards,
Robert Clifton
Hello Robert,
I am very thankful for your patient in helping me! Now I have a good news to tell you:
I find where the problem with TPA3250 and TPA3255. In another early version the problem does not happen because I connect /RESET and DVDD with a 100k resistance. In this two new evaluate board of 3250 and 3255, I leave /Fault pin float because I thought /RESET pin is internally pulled up.
I want a double check if a pull-up is compulsory and what are possible sollutions to make / RESET work stable.
I reviewed function of /RESET again and see that connecting it with DVDD is totally OK.
Another new question is: Can I connect /Reset pin with /FAULT or /OTW Pin directly to realize an auto-reset function when fault or overtemperature happens?\
Thank you!
Hi Louie,
I'm glad you were able to work passed this issue!
I see a potential concern with this auto-reset function. Let's say the fault occurs due to an over temperature. If you have an auto-reset the device will continuously turn back on and then shut off because there had been no time for it to cool off!
The over-current fault reporting is another Fault condition you wouldn't want to have it auto-reset on.
OTW pin also serves as a clip detection. So I wouldn't hook this up directly to RESET either as you will reset anytime clipping is detected!
Best Regards,
Robert Clifton