Part Number: PCM1792A
Other Parts Discussed in Thread: PCM1792
I'm planning to design a PCM1792 based dac. I want to know if the current output is sourcing or sinking current. I want to make a remove the voltage offset on the output of the ivc by connecting a current source/sink to the output of the PCM1792A. So basically I have two questions:
Is the PCM 1792A sourcing or sinking current?
Can I remove the offset voltage by connecting a current source/sink of 6.2mA to the output of the PCM1792A?
Best wishes,
Rogier van den Berg