This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3106EVM-K: Query the setting of TLV320AIC3106EVM-K

Part Number: TLV320AIC3106EVM-K


Dear Sir(s),

I'm working on TLV320AIC3106EVM-K, and I use I2C to connect the kit, send the below data to kit, but the configurations is incorrect when i try to read back,

1. hardware reset for pull down RESET for 1 ms.

2. delay 10 ms 

3. w 30 00 00

4. w 30 01 80

5 delay 20 ms 

6. w 30 02 00

7 w 30 03 20

8 r 30 02 20

9 R 30 03 04 

both the configurations of REG02 and 03 are not same as my setting, I do not know the reason?!

Please help me and best regards,

JBLIOU