Part Number: PCM9211
Hi Sir,
Pls kindly advise 2 questions as below, thanks.
Q1.
We use ARC (TV) continuous output music to soundbar, soundbar will have S/PDIF signal to PCM9211 RXIN3, then through Main output port to DSP.
We will also monitor register 0x38 and 0x39 Port Sampling Frequency Calculate Status; register 0x38 Calculate Status is “0:Calculated” ;
but sometimes will read 0x38 is “1:Calculating”, and music will discontinuous (ON-OFF-ON-OFF...).
For above issue, if what we can check something happen?
(Format is DD or DD+)
Q2.
When DIR using in wide mode (192K-Hz), if Register 24h/OSCAUTO need set to 1?
Thanks, Ian.