I wish to use the TLV320ADC6140 to sample two differential input signals, and I would like to configure the ADC to operate as the Master of the Audio Serial Interface. It is my understanding that I need to provide an external MCLK source to the device, is this correct? If so, can I connect MCLK to any of the unused GPIx inputs, or is there a specific pin that must be used?