Part Number: PCM1864
Hi All,
I am looking for an audio codec or processor that can perform a few functions and am wondering if the PCM1864 can do so.
I require 4 analog input channels (2 stereo inputs) and two analog output channels. We need to detect when two of the inputs have some audio input and switch to use those inputs. When those two inputs have no audio, we will instead use the other stereo input channels. We also require the addition of programmable filters, to remove noise and other unwanted audio. Finally, we require digital volume control and mono mixing capabilities.
Can the Energysense/Controlsense function of the PCBM1864 detect mic level voltage (around ten mV) on 4 inputs? If not, could you please recommend a product that can do this?
Thanks.