Part Number: TPA3255
Other Parts Discussed in Thread: INA253, TAS5614, TAS5634,
I was hoping to adapt the TPA3255 for use as a current source where I can take advantage of the amplifiers high efficiency, power and low noise attributes. I would be using the TPA3255 in a non-audio application. Basically I would like to use it to pulse (more like a triangle ramp-up and down) 10A of current through a coil that measures (~1mH and 2ohms). The "pulse" would ramp up to 10A within 1ms and then ramp down to 0A in ~500ms.
As a first pass design concept I was thinking of placing a TI INA253 current sensing amplifier after the output LC filter and feeding that back around to the input via an error amplifier. Does this sound reasonable?
Do you have any advice for attempting this (or alternate solutions?).