Other Parts Discussed in Thread: TAS3204, OPA1632
Hello TI community,
I'am new to the world of the TAS Audio DSPs and just finished my first board with the TAS3204. Now like almost always the problem is to get the chip running. The hardware is completed and from my understanding ready to be used. I'am using the analog in- and outputs of the DSP in combination with my selfbuild PA loudspeakers. What I have so far, is that the xtal is running with the correct frequency and I can see a signal on the clock outputs. Furthermore I'am measuring round about 1.8V at the VR_ANA, DIG and PLL pins. Then I tried to start the DSP in the I/O test configuration, which is described in the datasheet by using my system controller. After coming out of the reset the DSP consumes 180mA which should be within the specified limits and is communicating with the eeprom via the I2C bus. So far for me everything looks good, the problem is that I won`t get any output from the TAS. So I was thinking maybe the analog in- and outputs aren't routed in passthrough during I/O test configuration but I couldn`t find an answer to that in the datasheet. The next thing that came to my mind, that maybe the mute pin is active even if the datasheet says it won't, so I tested this with my system controller by pulling the mute pin to vcc or ground. Still no luck. After that I double checked my hardware. I found that VMID is just a litte above 200mV but since the datesheet won't tell me the nominal voltage I don't know if this is the normal condition. VREF is another unknow value for me I measured 1.3V but is it correct? Long story I know, so let me sum up my questions:
1. In I/O test configuration does the TAS3204 stream audio from the analog inputs to the analog outputs?
2. Is there a register that must be written to set the output volume of the DSP either in the test configuration or during normal operation to get output?
3. What are the normal voltages for the VMID, VREF and REXT pins?
4. Any other ideas to get the DSP working?
Yours faithfully,
Christopher