Part Number: PUREPATH-CMBEVM
Other Parts Discussed in Thread: TIDA-060026, TAS5825M, TAS5720M
The TIDA-060026 (TAS5825EVM-SB) shows a multi channel prototype setup where the PPC-MB is connected to one unit, then I2C and I2S are daisy chained to provide amp channels for all the various 9.1 outputs. This means that the PPC-MB must be receiving a multi channel audio stream. Typically this would be encoded information (Dolby or DTS), but I don't believe that the PPC-MB can decode this information. So with this in mind, I have 2 questions:
1. How are the 9.1 channels input into the PPC-MB
2. How are the channels then assigned to the various channels of the downstream modules (assuming they have individual I2C addresses).