Hi Team,
My customer is considering to use the TLV320ADC6140 as audio ADC with 384kHz sampling rate.
- Audio Signal Input Channel Configuration is Analog differential input.
- P0_R59_D[1:0] : ADC_FSCALE[1:0] = "00" (default) for DIFFERENTIAL FULLSCALE INPUT SUPPORTED = 2Vrms.
Electrical Characteristics of TLV320ADC6140 datasheet shows,
- Differential input full-scale AC signal voltage: AC-coupled input: Typ= 2 VRMS
Which one is the typical differential AC-coupled input rage?
a) (INxP - INxN) = -1.41V to +1.41V
b) (INxP - INxN) = -2.82V to +2.82V
c) (INxP - INxN) = 0V to +2.82V
Best Regards,
Koshi Ninomiya