This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2902C: PCM2902c Setup

Part Number: PCM2902C
Other Parts Discussed in Thread: PCM2900C

i want to use a PCM2900C  as a 16bit ADC ( The PCM2900C has an USB Port).

I need a stereo input at 44.1 kHz sample rate.

in the data sheet is discribed that i have to change the setting of Interface #2 to 0x03.

There are an software example  to set the PCM2900C.

My programming invironment ist LabView2019 from NI.

Exist an example for LabView 

Mit freundlichen Gruessen

Juergen Pfeifer

(stay healty)