Connect to 2.5mm jack with CTIA.
Is it okay if the OUTER- and OUTL- signals have the same GND connection?
Or does it have to be separated?
CTIAで2.5mmジャックに接続します。
OUTER-信号とOUTL-信号のGND接続は共通でも問題ありませんか? ・・・Common GND connection
または、分離しないといけませんか? ・・・Separate GND connection