This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6304Q1EVM: Stand-alone mode for TPA6304EVM

Part Number: TPA6304Q1EVM
Other Parts Discussed in Thread: TPA6304-Q1

Hello Team,

is it possible to use the EVM without using GUI to configure operation?

Means can this EVM be used in a stand-alone mode without PC? (with default register settings)

I think there is also access of the I2C pin on the EVM which can be connected to the target board of the customer?

Many Thanks

Josef