Other Parts Discussed in Thread: TAS5805M
Hi team,
My customer is evaluating a new design for their amp design.
Their previous is usually using our TAS5782m,
The existing new case will use 5W per channel stereo speakers,
PDVV may fall between 11 V ~ 19 V, the speaker may be between 4 ~ 8 Ohm,
Using TAS5782 according to this condition seems to be a bit higher. Please recommend other models of Amp.
The built-in DSP must contain at least the following functions:
1. Bass Mono Mixer
2. EQ above 10 bend
3. DRC
4. AGC / AGL
5. Spatializer
Is there any other option with lower output power than TAS5782m and relatively low price? Thanks.