This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255: THD+N of TPA3255 from datasheet

Part Number: TPA3255

Hi

 I would like to know if the THD+N from the datasheet of TPA3255 was taken from EVM or with a direct connection to the XLR inputs (so bypassing the front end/opamp of the EVM)

  • Hello user, 

    The THD+N measurements are taken on the EVM with these conditions: 

    All Measurements taken at audio frequency = 1 kHz, PVDD_X = 51V, GVDD_X = 12 V, RL = 2Ω, fS = 450 kHz, ROC = 22 kΩ, TC = 75°C, Output Filter: LDEM = 10μH, CDEM = 1 µF, MODE = 10, AES17 + AUX-0025 measurement filters, unless otherwise noted.

    Most audio analyzers will not give correct readings of Class-D amplifiers’ performance due to their sensitivity to out of band noise present at the amplifier output. AES-17 + AUX-0025 pre-analyzer filters are recommended to use for Class-D amplifier measurements. In absence of such filters, a 30-kHz low-pass filter (10 Ω + 47 nF) can be used to reduce the out of band noise remaining on the amplifier outputs.

    All the best, 

    Carolina 

  • Ok but the signal was feed direct to TPA32xx or did it pass through the opamps

  • Hi user5327551,

    We don't use the EVM for the graphs in the datasheet. That requires a dedicated board for testing. This board does not have the opamps on the front end. We want to make sure to show the THD+N of just the TPA32xx device and not any other devices. 

    Regards,

    Robert Clifton