This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3118D2: Max output power for PBTL into 4 Ohms load

Part Number: TPA3118D2

Figures 22 and 26 provide the max output power graphs for PBTL into 2 Ohms and 3 Ohms.

Is there a graph for 4 Ohms PBTL?

Or what is the max output power for this condition:

1. PBTL

2. 4 Ohms

3. Vin = 22V

4. THD+N at 1% & 10%