This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2563: TAS2563 SDOUT

Part Number: TAS2563

Hi Guys,

My customer will using SDOUT for AEC reference.

What register need to set it up for SDOUT output?

Thanks, Ian.

  • Hi, Ian,

    Our team will take a look at this and will answer as soon as possible.

    Best regards,
    Luis Fernando Rodríguez S.

  • Hi Ian,

    Echo reference data is controlled by register 0x0C
    • Bit 6 enables (logic high) or disables (logic low) the data transmit
    • Bits 5 to 0 select the slot to send the data

    The slots are 8 bits long, this means there are 32 slots of 8-bits each instead of 8 slots of 32-bits each.

    Make sure to select Audio In & Audio Out at the End System Integration (this is default selection)

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators