Part Number: PUREPATHCONSOLE
Other Parts Discussed in Thread: TAS2557EVM
Hi
I have one problem with TAS2557EVM and PPC3 v3.0.8.
I have made EQ-tuning and I'm tryin to do DRC tunings. I feed very low level Pink noise signal from pc via USB to the EVM board. First I have only EQ ON and DRC Off. Frequency responce is as it should be. Then I put DRC ON with compressions are 1:1 in all bands (700Hz, 700z to 6000Hz and 6000 Hz). DRC should not be affected at all. BUT frequncy responce is attenuated at higher end.
DRC OFF:
DRC ON:
Here are DRC settings:
What can cause this kind of effect?