hi,
i am working the below attached circuit for my input voltage range of 9mV to 14mV so that i can get the output from 0 to 2.7V . i am feeding 10mV at the input,the output is oscillating from .5 to 1V which i have observed in scope.i dont know why.please confirm if my New Doc 2020-05-27 14.32.03_1.pdfcircuit and thNew Doc 2020-05-27 14.32.03_1 (1).pdf