Part Number: TPA3132D2
Hi Team,
If we want to estimate input power current consumption under a given use condition, please help me to check if my calculation looks ok or not, thanks!
PVCC = 24V
Output = 18W
Load = 4 ohms
THD <= 1%
Mode = BTL
Assume Gain = 20 (dB)
Assume efficiency is 90%
Assume we use input divider to limit input voltage to 0.9 Vrms
No additional PLIMIT
Calculation:
Eff is 90%, so PVCC power consume 18W / 0.9 = 20W
Peak power = 20W * 1.414 = 28.28W
PVCC = 24V, IVCC = 28.28W / 24V = 1.178 A (pk) -> this is for output 18W
Assume quiescent supply current = 30mA at PVCC = 24V
Total current consumption is 1.178 A + 30mA = 1.208A (pk)
Is my calculation sounds ok to you?
Thanks.
Andrew