Other Parts Discussed in Thread: TPA3255, , TPA3244
Hello,
I'm searching for the TPA3245EVM Gerber data, but I was only able to find the data for TPA3244 and TPA3255.
Is there a Gerber data for TPA3245EVM?
Thank You
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm searching for the TPA3245EVM Gerber data, but I was only able to find the data for TPA3244 and TPA3255.
Is there a Gerber data for TPA3245EVM?
Thank You
Hi Sam,
Thanks for the data!
I just have one more question regarding the EVM schematic.
I checked that the most of the TPA32XX series amplifiers have the high current shunts parallel to the capacitor at the output.
I'm planning to use my amplifier in BTL and PBTL mode settings, so from the user's manual, I don't have to remove the shunt resistors from my EVM.
I don't need any current measurements for my purpose, so will my EVM board work fine without the serial capacitors and shunts all together? (C21, C34 capacitors n the diagram below)
Hi,
The shunts and capacitors you mentioned was for BTL/SE configuration. If you are using BTL, just remove the capacitor and the shunts, and connect the OA and OUTA together. Thanks!
Regards,
Sam