Hello,
I'm using the PCM2912A with the amplifier TPA6111A2DR.
On the VDD pin I'have 3.1V and not 3.3V. Also the PCM2912A it is a little bit hot and the current consomption it is a lit bit more than the EVK.
I think the problem it is perhaps the use of the TPA611A2DR.
I put the in attach file the schematic of my board.
best regards
David Laurentdesign1.pdf