Hi.
I would like some clarification about the header file generated by the dump process inside PCC3 needed to initialize TAS5805M.
Should I to dump each component even though I don't use it? Or could I dump only the active ones?
By now I am using the complete dump but as I only need the AGL/OTFB optional component, I would save a lot of memory in the MCU if I could use the partial dump.
Related to the AGL/OTFB component, I also would like to confirm with you that I must enable the AGL to make OTFB work, mustn't I? Even if I don't really need the basic AGL feature and I don't modify any of its default parameters (AGL Threshold = 0). Or is there any way to make OTFB work without enabling AGL?