Other Parts Discussed in Thread: TAS2560
Hello,
Regarding to USB interface on TAS2560 EVM, my customer is asking some question.
They will output from USB audio (PC).
.(Question)
1) When USB audio is fs=48k.16bit format, can it output to speaker without PPC3?
I think it seems it can output on standalone from EVM manual.
If possible, can it be suppored on Win10?
2) When they will use PPC3, how procedure do they need to output from USB interface?
They set as following but didn’t output.
・Connect EVM to PC(USB) and run PPC3
・SystemChecks -> AudioModeSelection(select ROMmode2) -> AudioPlayer
Is their procedure correct? Do they need to consider some point as output?
They confirmed the EVM is recognized as USB-AudioEVM on device manager..
Regards,
Tao_2199