Hi,
Good day. I hope everything is fine.
Our customer is looking for two audio amplifier that would fit in the requirements below:
1) to drive 3 8ohms/15W treble frequency loudspeaker, each loudspeaker is different channel;
2 IIS input
THD+N<1% when output power is 15W
THD+N<10% when output power is 30W;
Sample rate >= 96khz
SNR>100DB
2):to drive 1 8ohms/60W subwoofer;
THD+N<1% when output power is 120W
THD+N<10% when output power is 200W;
Sample rate >= 96khz
SNR>100DB
I would really appreciate if you could help us suggest a product that would fit with these requirements. Thank you and have a great day.
Regards,
Cedrick