Hi,
My customer wonder if the PCM1862 can support 24.576MHz bit clock as slave, and tolerate a longer frame sync interval than usual?
Here is the scenario:
Fs = 48KHz
Wl = 24bit
Mclk/Sclk = 24.576MHz from Master
Bclk = 24.576MHz from Master
Wclk = TDM16 Frame = 512 x BCLK (TDM16 = 16X32bit)
It is OK if the first two TDM slots are used for data transmission, but it should wait nicely in Hi-Z until start of next frame, 512 bitclocks later.
Thanks.
B.r M.A.M