This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5825P: Missing register definitions for a commonly used slider in PPC3

Part Number: TAS5825P


Hi, I left a feedback on the SLASET9 document as well, that there are two registers which seem to be one of the most important ones adjusting volume 0x0c and 0x10, that are missing documentation in the datasheet, but those are the two registers in the i2c monitor in PPC3 getting 5-byte write bursts when the volume slider is adjusted between +48dB and -110. PGA and AGAIN registers have no similar effect than this single slider alone. 

Could you please share the register definition for those two?

Thanks