This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC6140: TLV320ADC6140 & ADC6140EVM-PDK Setup & Comparison to PCM1865

Part Number: TLV320ADC6140
Other Parts Discussed in Thread: ADC6140EVM-PDK, , PCM1865, OPA1664, OPA1654, OPA1604, OPA1612, OPA1656, OPA1692, PGA2500, PGA2505

A couple questions on TLV320ADC6140 and ADC6140EVM-PDK.

1. I am currently using 2 x PCM1865 in a design for capture of 8 microphone signals. Is the TLV320ADC6140 considered an upgrade? I am not interested in DRE as it could effect array performance and sound localization, so it seems max DR with PCM1865 is 110 dB while TLV320ADC6140 is 113 dB. In addition, TLV320ADC6140 can support 32-bit output and more. Any further comment on if PCM1865 will be NRFND and will be replaced by TLV320ADC6140?

2. I am not using TDM mode with my 2 x PCM1865 setup. CH1-2 → DOut1 and CH3-4 → DOut2 (GPIO setup like this). So 2 separate I2S lines each with 2 channels for each PCM1865. Can ADC6140EVM-PDK setup like this for testing? I only see mention of TDM. I would like to support 8 analog microphones 32-bit / 192kHz using 2 x TLV320ADC6140  as I have previously done with PCM1865 using 2 DOUTs per chip. Any issue?

Any other comment on moving from PCM1865 to ADC6140EVM-PDK (pros/cons) is welcome. Thanks!!

  • Hello,

    Nice name!  

    1.)  Glad you like the TI Audio ADC offerings, including our newest ADC6140 device, which in many ways is an upgrade to the PCM186x family.  We really recommend you give the DRE a try, the feature is used in several active voice activated systems on the market and our understanding is that those systems use advanced beamforming algorithms to help with the voice processing.  

    There are no plans to obsolete or NRND the PCM1865 device per TI standard policies. https://www.ti.com/support-quality/quality-policies-procedures/product-life-cycle.html

    2.)  Yes, you'd be able to wire up the ADC6140EVM-PDK to work in this manner by connecting the appropriate external ASI signals to the bottom male headers on the AC-MB board and then selecting "External ASI" with the DIP switches.  The USB streaming features are fixed to TDM protocols on the EVM.

    No issues having 8x32-bit outputs using 2x TLV320ADC6140 devices.  Note that there are some processing block limitations while operating at the increased sampling rates as described in detail in this application note:

    https://www.ti.com/lit/an/sbaa381/sbaa381.pdf

  • Hi Collin :)

    Thanks so much for the insight — very helpful. I will give DRE a try at the lower sample rates.

    A couple more questions comparing the two chips:

    1.) Is there a similar chart of ADC6140 Figure 13 (Input-Referred Noise vs Channel Gain) for the PCM1865 ? Can you comment on noise for the two chips? Along with the built-in PGA, I am using OPA1664AIPWR + digipot for programmable front end mic gain, sensitivity matching and differential signal drive before PCM1865. In this way, noise performance is optimized for my electret mic capsules. Should I expect to use a similar front-end again with ADC6140 after taking into account changes for the lower full-scale input?

    2.) If so, out of curiosity, are there any other front-end opamps you would recommend for this purpose (The OPA1692IDGKR looks good, but I don't believe it comes in a quad package)?

    Thanks again for your help!

    Colin

  • Hello,

    1.)  We don't have the requested data available for the PCM186x, but since the input range is higher yet the performance is the same, we can infer that the input referred noise of the ADC6140 is lower.  

    Are you operating with very low-level signals from the microphones?  It's not very common that an external gain stage is required with these devices, but it may be doing a SE-to-DE (or vice-versa) conversion before it reaches the device.  

    Additionally, the ADC6140 features fine gain and phase adjustment capabilities which may also eliminate the need for the external adjustment requirements.

    2.)  We can certainly help recommend an external amplifier, but would still like to confirm that one is required.  Is it for a receiver or signal conversion stage, or is extra gain really required?

  • Capsule noise floor is 16 dB-A and there are plenty of folks trying to capture nature sounds where that can become a problem, as they apply lots and lots of gain at capture and in post. Since I also want to capture sounds up to 136 dB-SPL, I use the front end to accommodate large gain changes, while the PGA in the PCM1865 provides finer control. Yes, this is doing SE to DE conversion before PCM1865. The front end also stores sensitivity calibration.

    The gain and phase adjustments got me excited, but in practice a gain calibration of -0.8 to 0.7 for analog capsules is not enough. I know it can be for MEMS and some PDM mics, but not the higher SNR analog capsules I've seen, where sensitivity tolerance is commonly +/-3 dB at 1 kHz. The fine 0.1 dB resolution could be helpful, however!

  • Fair enough, thank you for the additional information about the desire to further increase dynamic range of the front-end.  

    OPA1604 is our lowest noise quad, with OPA1664 in 2nd.  The OPA1654 is a good quality CMOS offering as well.

    There are more choices in dual-channel and the OPA1612 is our flagship with the lowest noise/distortion available.  OPA1656 and OPA1692 are also good offerings.

  • Collin, Thanks so much for your time — I appreciate the review of my approach and will look at the opamps you mention.

  • You're welcome!

  • I have the ADC6140EVM-PDK here now and am evaluating. I missed the part in the datasheet where it says you cannot change the analog PGA gain once the device is powered up — something I suppose I took for granted with the PCM1865.

    So, am I correct that you cannot monitor signal level while changing analog gain or when using the phase and gain calibration? If so, how does one go about using the calibration features without monitoring signal?

  • To follow up my questions from yesterday:

    If I can't use the internal analog PGA when the ADC6140 is in active mode, is there a TI part you can recommend that could potentially do this as an integrated digitally controlled front end? Noise from zero-crossing on gain change is a concern here and the typical PGA2500, PGA2505 seems like overkill, since I would need 8 of them ($$$) and don't need the higher voltage rails. These parts look to be aimed at ultra-sound, but would any be worth looking at for audio in my application?

  • Hi Colin,

    It is actually possible to change the channel gain on-the-fly with TLV320ADC6140! The preferred method would be to use the digital volume control which supports a range of -100dB to +27dB with 0.5dB steps. This gain change happens seamlessly with built in soft-stepping so there are no audible artifacts introduced. Note this is separate from the PGA gain and happens after the conversion in the digital processing blocks.

    If this is not sufficient, it is technically possible to change the PGA gain on-the-fly as well, but there is no zero-crossing detection or soft stepping applied between gain levels so this may cause audible artifacts for a short period of time (typically up to a few 100us). This is why we don't fully support this mode, because it is possible, but the device is not optimized to do this. The GUI does not allow you to do this since we do not highlight this as a feature, but you could use the I2C monitor within the GUI to write the registers directly and observe the response to see if the behavior is okay for your application.

    If you feel that the digital gain is not sufficient and the artifacts from changing the PGA gain on-the-fly are too significant, then I think your best choice would be to stick with the PCM1865. As Collin mentioned there are no plans to NRND this device and it is still a high performance device in the portfolio. It does use zero-crossing detection when making on-the-fly PGA gain changes so it will not introduce these artifacts.

    Best,

    Zak

  • Zac,

    Thanks so much for the additional information about gain staging and control — super helpful. Any comment on Texas Instruments PGA/VGA parts for audio use? For example, would they have audible artifacts on gain change?

    Thanks,
    Colin

  • Hey Colin,

    Happy to help! I don't have any experience with our PGA/VGA parts myself though so if you would like to explore that option I would suggest making another thread with one of those part numbers so it gets to the right people!

    Best,

    Zak