Are there any rf issues with using longer speaker wires in the 50 - 150 foot range
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tom,
Could you please tell us your case application? PVDD, load, and output power.
Regards,
Derek
we have 5 small video viewing room in a row. each is 5.1 audio. Im doing a monitor control for them and would like to put the power amps in the same box. the 5 speakers are 8 ohms, peak power is maybe 10 - 15 watts, average seems to measure around .9 watts per channel the 3 mains have approx 18 feet of wire, the 2 surrounds are about 40 feet. There are several video monitors, computers and scopes in each room plus the audio monitor control. . I was thinking of going to the class D amp instead of the AB just for the lower heat. But if RF is an issue I will stay with the Class AB.. it would be 30 of these amps in about 50 feet of hallway
Hi,
If long cable application, I suggest adding inductor and beads on output. It will be better for EMI performance.
Regards,
Derek