This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sirs,
We are designing the TPA6166 with an OEM customer. Here we have two questions which need product line's support:
1. WOuld you please advise if the TPA6166 detect OMTP and CTIA jacks based on the same impedance range of the TS3A227E device?
TPA6166 datasheet:
TS3A227E specification:
2. Can we bring up the TPA6166 to support OMTP/CTIA jack detection function with the following I2C instructions?
-----------------------------------------------------------------
w 80 1E 19 #Enable Registers 3
w 80 04 EE #Interrupt Mask Register 1
w 80 05 F4 #Interrupt Mask Register 2
w 80 07 B9 #Left Headphone Volume Register
w 80 08 79 #Right Headphone Volume Register
w 80 09 47 #Microphone/Ground Control
w 80 12 01 #Reserved Registers
w 80 13 45 #Reserved Registers
w 80 1A 95 #Jack Detect AC Test Settings
w 80 1E 01 #semi auto mode
w 80 1D 80 #Enable Registers 2
-----------------------------------------------------------------
Thank you and Best regards,
Wayne Chen
07/16/2020
Hi, Wayne,
The TPA6166A2 can support both jack connections in the impedance ranges that you showed in the pictures.
Regarding the registers configuration, it seems to be all in order. I didn't find anything that should be modified or added.
Please let me know if you have additional questions or comments.
Best regards,
Luis Fernando Rodríguez S.