Part Number: PCM2903C
Other Parts Discussed in Thread: PCM2903
Hi team,
I was looking at the reference design for the PCM2903 Audio Codec, and the VIN coupling caps are electrolytic caps. Are these required, or can they be ceramic caps?
Thanks,
AH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Yes, the input capacitors can be ceramic. When the EVM was released it was harder to get decent dielectric ceramic capacitors, but that has changed since. You should try to use a larger value capacitor with a voltage rating at least double the rated working voltage to help minimize low frequency distortion. Film caps will be the highest performance but are likely not required with the PCM2903.