Part Number: LM4562
Hi TI team
I would use the LM4562 in my "balanced control volume" project. I have several stages for each channel, so I'm using 5 chips in total. The board will have +15/-15V generated with LM7815/7915.
For LM4562 chips, on each power pin (VCC and VEE) I would use very close to the pin a X7R cap in parallel with an electrolitic cap to reduce the noise.
My question/doubt is about the value of these caps. On the chip datasheet there are 2 different diagrams. In figure 110 there is just one cap of 47uF on each power rail. Instead in figure 113 there are 2 caps in parallel one of 10uF and one of 0.1uF.
So my question is which are the right values to use?
What happen if I use bigger caps? For example 100uF and 0.47uF?
Thanks
Giuseppe