This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS3251: TAS3251 Questions.

Part Number: TAS3251

Hi Sir,

My customer using TAS3251 for 100W, (VDD=26V @ RL=2ohms),  here are 2 questions need your help, thanks.

1. What is min. o/p inductor? 4.7uH or 2.2uH or...

2. TAS3251 will default active w/o initial setting?

Thanks, Ian.

  • Hi Ian,

    Usually, the smaller inductor is, the larger ripple current is. Can you share the background of customer's requirement for the minimum inductor?

    As tot the initial settings for TAS3251, it is suggested to grant you and customer the access to TAS3251 in PPC3 GUI and then customer can generate the settings from PPC3 software.

    Please let me know your thinking, thanks!

    BR

    Alix Wan.

  • Hi Wan,

    1. can it using 4.7uH or 2.2uH? (small inductor reduce space)

    2. Can it active w/o setting? (default active)

    Thanks, Ian.

  • Hi Ian,

    1. As you know, the LC filter in a class-d circuit is used to filter out the switching frequency components. 4.7uH can be used, but that may lead to insufficient attenuation on the switching frequency components and degrading the audio performance.

    2. Yes, by default it should be active.

    Thanks!

    Regards,

    Sam

  • Hi Ian,

    Furthermore, small inductance may lead to high inductor current ripple, degrading the audio performance and also easier to trigger the OC fault when outputting high power.

    Thanks!

    Regards,

    Sam