Part Number: TPA2008D2
Hi Team my customer is having an issue as described below:
With 3.6Ohms speakers connected to each output of the TPA2008D2 part (one per channel) and the volume set to 60% and above they see that the speakers make a quick sound but then rapidly turn off. Once this happens, sounds cannot be played through the monitors/speakers until power is cycled on the monitors.
Questions:
- They have switched to connecting both speakers in series and driving them with one output of the TPA2008D2. Do you see any issue with this? This may have fixed our problem, but they are getting some reports of intermittent issues that might be related.
- It looks like we may be hitting the short circuit protection circuitry of the TPA2008D2.
- What is the current level to trip this short circuit protection?
- How long of a duration short circuit will trigger the protection?
- Does is trip instantaneously or does the over-current need to persist for some amount of time?