I am trying to use 2 pair of master and slave (4 boards) to allow bidrectional audio communication, 1 master and slave board on each end. However when i turn on the boards one of the master slave pair loses/has a flaky connection, led D9 starts blinking. Is this setup possible and if so do i need to change something in the network pairing to make it work?