This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC24K: Grounding scheme for audio codec

Part Number: TLV320AIC24K

Hi, 

We are using three TLV320AIC24KIPFBG4 audio codecs in cascaded mode on our board with microphone input and 150 ohms audio outputs.

We are referencing these audio codecs to digital ground since we do not have separate analog ground on the board. 

 

We cannot meet the datasheet recommendation (as shown in below snapshot) on our board. 

  • Is it necessary to keep two separate grounds (AGND and DGND) for this codec?
  • What would be the impact of referencing audio codec to digital ground considering that there is no possibility of having a separate analog ground?

 

Awaiting for your response.

Regards,

Archana Rao

  • Hello Archana,

    I did not see an attached picture. Can you please resend this?

    Connecting AGND pin to DGND plane directly may cause some external noise to be introduced as DGND is usually the more noisy of the two. Ideally, the AGND and DGND ground planes should be separated on the board and should be shorted at only one place as close to TLV320AIC2x as possible. 

    Regards,

    Aaron

  • Thank you for your reply, Aaron!

    Please see the image below,

    What would be the impact on analog codec operation if DGND noise gets coupled to it?

    Since, we have no provision of AGND on board, we are forced to reference audio codec to DGND.  We really need clarification on this perspective for the deviation taken.

    Regards,

    Archana Rao

  • Hello Archana,

    Sure thing! It is honestly hard to say exactly what the impact will be. Ultimately, noise from DGND can get coupled in the analog portion and make it's way to the analog inputs of the device and degrade performance. 

    In order to prevent this, we highly recommend following data sheet recommendations. 


    Regards,
    Aaron