Part Number: TAS6424LQ1EVM
Good Day,
I have the TAS6424L Eval Board and PurePath Console application. I want to configure the IC through the USB cable. I have connected the power supply and the speaker to the output. Also arranged the Channel 1 to the play mode.
I truely do not understand where should I give an input audio signal. In the user guide of eval board, it is written that "If USB is selected, Windows Media Player can be used to stream audio." and "The audio can be streamed now to the speakers. Go to the GUI and click on “Device Monitor & Control” box. Click on play button located on the top right of the window." But as you can see below, I do not have a "play button" anywhere. Is there anything missing? or Is there anything I can't see?
I appreciate for your all help. Thanks.
Best Regards,
Amine