This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3140: How many bits of ADC resolution does this device capture?

Part Number: TLV320ADC3140


Oddly, I can't find this information in the datasheet or product listing. How many bits are converted from the output of the PGA?

I am using the TLV320ADC3140 to capture audio at sample rates of up to 96kS/sec, to be saved in a .WAV file. Hence, I am reading out 16-bit samples from the serial interface. I had assumed that 16-bits is also the resolution of the ADC, which seems typical for this class of device.

Here's the confusion: If I apply 6-dB of digital gain,  that should effectively shift the data word one bit to the left, so the LSB would always be 0. With 24dB, the 4 LSBs should be 0. Yet this is not what I see happening, so clearly the device is capturing more bits internally than it is outputting. My question is how many bits are being converted?

Thanks.

  • Hi David,

    The TLV320ADC3140 can be configured for a word length of 16, 24, or 32-bits. The typical SNR for this device is 106dB, which means the effective number of bits (ENOB) is 17. The remaining bits are not masked though so you can expect them to toggle randomly with noise rather than remain static.

    Best,

    Zak