Other Parts Discussed in Thread: CC8520
Hi,
I am trying to program 8520 using i2c. I am able to program the eeprom and read out the correct data from memory. But when I power in the 8520 module the module is trying to read the data from the memory but doesnt load the application.
I wish to know some clarifcation on i2c format described in manual. In DWC field : what will be the flash image look like. Are we expected to consider the DWC (2 bytes) + CMD (2 bytes) + data (32K bytes from purepath) + CRC (4 bytes) as final value in DWC. Also what is the byte format for DWC and CMD (MSB first or LSB first). Also I am confused with Data + CRC field. Are we required to add 4 byte CRC at the end of the 32K data because the data already includes CRC.
I am expected an example how the i2c memory format (first 4 bytes and 4 last bytes) will look like in practice for purepath Application Master mode(32K Application).
RBG