This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5421EVM: DC offset fault

Part Number: TAS5421EVM

Hi Audio Expert, 

I am evaluating TAS5421EVM. the final application is to use it to drive a transformer, which may have a core saturation problem by the application note. before I connect to the transformer, I try to use a 56ohm, 1/2 W resistor to check the platform. 

power is 12.2V, the input is 50mV 1KHz sine wave,  default gain of the evaluation board I think is 26dB. I kept having DC offset shutdown fault condition.

I connected two scope probes to the electrode of the load and ground.  You can see yellow trace is OUTN, blue is OUTP. pink is the input. the input is single-ended, I shorted the R6 on the EVM board.

did I do something wrong or the board got damaged?

Thanks,

David Sun